Solution
Press Load Monitoring
Press forming is a method to deform different materials. For instance, materials such as steel can be bent, stretched, or formed into shapes.
Press forming is a method to deform different materials. For instance, materials such as steel can be bent, stretched, or formed into shapes. A force measurement solution is required to monitor the forces being applied by the press forming machine. This ensures quality control and traceability during the production process.
For large press forming machines, Interface recommends installing the 1000 High Capacity Fatigue-Rated LowProfile™ Load Cell. When the material is placed under the punch plate to form a shape, the force applied is measured by the 1000. The force results captured is sent to the INF-USB3 Universal Serial Bus Single Channel PC Interface Module, where results can be graphed and logged on the customer’s PC with provided software.
Interface’s force measurement products and instrumentation accurately monitored and logged the force results of the press force machine, ensuring zero-error production performance.
Notifications